EcoStruxure™ Control Expert - Flow Calculation Library

Flow Calculation Library
Published by Schneider Electric

Overview

EcoStruxure™ Control Expert - Flow Calculation Library
EcoStruxure™ Control Expert Flow Calculation Library includes advanced reporting standards for different reports based on the AGA standard.

The following AGA gas reports are supported by the library:

  • AGA3: Orifice Meter Gas Calculation
  • AGA5: Calculation of Gross Heating Value, Relative Density and Compressibility Factor for - Natural Gas Mixtures
  • AGA7: Turbine Meter Gas Calculation
  • AGA8: Compressibility Factor Calculation of Natural Gas and Related Hydrocarbon Gases
  • AGA9: Ultrasonic Meter Gas Calculation
  • AGA11: Coriolis Meter Gas Calculation
  • VCONE: V-Cone Meter Gas Volumes
  • Compatible with : Control Expert V8.0 and above

    EcoStruxure™ Control Expert - Flow Calculation Library

    Details