AVEVA™ Predictive Analytics

Early warning notification and equipment diagnosis application
Published by AVEVA Group PLC

Features

  • Alerts and Notifications
  • Data Analysis
  • Monitoring and Diagnostics
  • Calculation Engine
  • Transient Module
  • Security

Alerts and Notifications

  • Set alert thresholds to communicate when the deviation between actual values and predicted values exceeds allowed limits.
  • Manage alerts in a variety of ways including by alert category, level, criticality, duration, and frequency
  • Alert events directly linked to a graphical trend showing the event data, threshold limits, and times when the values are in alarm mode
  • Relevant users and groups can be notified in real time if an asset is in alert status through AVEVA™ Predictive Analytics's customisable email notification capabilities
  • Data Analysis

  • AVEVA™ Predictive Analytics includes a variety of advanced statistical and model-based comparison applications and business intelligence tools that enable users to spend less time searching for potential problems.
  • Users have the ability to view the raw training data, see results of the model, compare the performance of similar assets of the same type, and view the effects of alerts.
  • Diagnostic ability reduces the likelihood that an engineer will attribute abnormal operating conditions to the wrong variable.
  • Monitoring and Diagnostics

  • AVEVA™ Predictive Analytics offers comprehensive monitoring and diagnostic services remotely on-site. We can train you to deploy, maintain and monitor your own models, or we can do the monitoring for you.
  • Our team of experienced engineers can assist you with every step of the process from model training, to diagnostics, to best practices.
  • Calculation Engine

  • AVEVA™ Predictive Analytics software includes an advanced calculation engine that provides the ability to develop simple and complex calculations to create pseudo or ‘virtual’ points
  • Results of calculations can be used in PRiSM Predictive Asset Analytics models, allowing for greater system flexibility
  • Calculations can automatically back-calculate, making historical data available for the monitoring period before the current calculation was created
  • Transient Module

  • AVEVA™ Predictive Analytics Transient Module provides the ability for online monitoring of abnormal conditions during a transient, such as startups and shutdowns
  • The solution is also able to automatically identify previous transient events from the historian, which is useful for comparisons
  • Security

  • AVEVA™ Predictive Analytics software integrates with existing enterprise security systems. The system supports single sign-on authentication, and administrators have the ability to limit user access rights and editing privileges at a granular level
  • Unauthorised background image

    Your product is just steps away!

    Register for FREE to buy, get downloads and access free trials.

    Get Resources and Start FREE Trials

    Easy Product Activation with Your Account

    Products Saved to Personal Digital Library