Smart Connector - Pelco VideoXpert ASCII Interface
Extension allowing connection between EcoStruxureâ„¢ solutions and Pelco VideoXpert
Published by
Schneider Electric
Smart Connector - Pelco VideoXpert ASCII Interface
Published by
Schneider Electric
Features
Highlights
The Pelco VideoXpert ASCII Integration Services enables 3rd party applications to register events, which can trigger actions on the CCTV system. This integration enables alarms sourced in EWS systems to be parsed and presented, to the CCTV system. This can be used to create cause and effect scenarios, where BMS and its associated integrated systems can send events to the CCTV system to trigger camera positioning, film recording, scenarios and video layouts, and more.
Highlights
The Pelco VideoXpert ASCII Integration Services enables 3rd party applications to register events, which can trigger actions on the CCTV system. This integration enables alarms sourced in EWS systems to be parsed and presented, to the CCTV system. This can be used to create cause and effect scenarios, where BMS and its associated integrated systems can send events to the CCTV system to trigger camera positioning, film recording, scenarios and video layouts, and more.