SmartSense
Features
Highlights
Miniumum sensors. Maximum data.
SmartSense ‘Power Genome’ ensures early detection of machine degradation, using the least possible sensors
Reliable algorithms
Reliable algorithms built and enhanced using 4.1 TB data over 7 years
Brand agnostic
AI and ML models use Data + Domain, making the solution Brand Agnostic
Asset coverage
Covers a wide set of assets such as motors, transformers, chillers, pumps, compressors, escalators and elevators
Strong acquisition layer
Has a strong acquisition layer which is retrofit with 200 types of sensors, 12 Industry protocols, and enables 3rd Party Integration with SAP, BMS and other IoT Platforms
Proven solution
Proven solution which enables over 4000 equipment being analyzed using Power Genome
SaaS model
SaaS Implementation in an Opex Model, with minimal upfront investment
Key Offers
You will be granted access to the following resources:
SmartSense for digitization: Offers real-time asset monitoring
SmartSense for energy efficiency: Helps reduce cost of power through energy analyses & network leakage identification, along with root cause & recommendations
SmartSense for Predictive Maintenance: Helps reduce asset downtime and maintenance costs by identifying asset degradation, along with root cause & recommendations
Highlights
SmartSense ‘Power Genome’ ensures early detection of machine degradation, using the least possible sensors
Reliable algorithms built and enhanced using 4.1 TB data over 7 years
AI and ML models use Data + Domain, making the solution Brand Agnostic
Covers a wide set of assets such as motors, transformers, chillers, pumps, compressors, escalators and elevators
Has a strong acquisition layer which is retrofit with 200 types of sensors, 12 Industry protocols, and enables 3rd Party Integration with SAP, BMS and other IoT Platforms
Proven solution which enables over 4000 equipment being analyzed using Power Genome
SaaS Implementation in an Opex Model, with minimal upfront investment
Key Offers
You will be granted access to the following resources:
SmartSense for digitization: Offers real-time asset monitoring
SmartSense for energy efficiency: Helps reduce cost of power through energy analyses & network leakage identification, along with root cause & recommendations
SmartSense for Predictive Maintenance: Helps reduce asset downtime and maintenance costs by identifying asset degradation, along with root cause & recommendations