EPLAN Smart Wiring
Published by
EPLAN
Features
Increased efficiency
EPLAN Smart Wiring is a SaaS based solution for optimising the processes in manual control cabinet wiring.
Simple, clear and touch-optimised user interface, for use on mobile devices
Integrated data and processes from engineering through production planning to production
Wiring without schematic
Step-by-step instructions for the panel builder
Automatic project comparison in case of last-minute changes
Creation of error messages and manufacturing protocols, including shipping, via email
Allows the use of less well-trained staff in the control cabinet wiring
Improved scalability of resources in production
Increased efficiency and sustainable reduction of costs
Wiring without schematics
Wiring is possible even without the schematics, which are stored in the assistant. For checking and reference purposes, you can access the schematics – starting from each individual connection.
Clearly visualized wiring
Easy-to-read visualisation of mounting layout, devices, connections, connection types and wire routing.
Automatic project comparison
If there are last-minute changes, you can perform an automatic project comparison to avoid errors. You can forward any anomalies directly to the engineering department via e-mail.
Clear monitoring – Even for wiring control cabinets in parallel
Project data are provided from a central server to enable identical control cabinets to be manufactured in parallel and for several wiring technicians to work simultaneously. Status information makes it easier to handover projects between different employees and to monitor a project’s progress.
Increased efficiency
EPLAN Smart Wiring is a SaaS based solution for optimising the processes in manual control cabinet wiring.
Wiring without schematics
Wiring is possible even without the schematics, which are stored in the assistant. For checking and reference purposes, you can access the schematics – starting from each individual connection.
Clearly visualized wiring
Easy-to-read visualisation of mounting layout, devices, connections, connection types and wire routing.
Automatic project comparison
If there are last-minute changes, you can perform an automatic project comparison to avoid errors. You can forward any anomalies directly to the engineering department via e-mail.
Clear monitoring – Even for wiring control cabinets in parallel
Project data are provided from a central server to enable identical control cabinets to be manufactured in parallel and for several wiring technicians to work simultaneously. Status information makes it easier to handover projects between different employees and to monitor a project’s progress.