ROMeo Process Optimization

Rigorous Online Modelling with Equation-Based Optimisation
Published by AVEVA Group PLC

Overview

ROMeo Process Optimization

ROMeo is the only complete process optimization solution that integrates heat and material balance rigorous simulation, data reconciliation, gross error detection, economic optimization, and performance monitoring into a single user environment.

Its online modeling and optimization capabilities utilize industry proven thermodynamic methods and data to generate highly accurate operating information enabling managers to react quickly and precisely to changes in market pressures, energy costs, and equipment performance.

ROMeo’s integrated interface and drag-and-drop functionality minimizes the user’s learning curve and accelerates real economic benefits. Its equation-based optimization engine is unmatched in modeling large processes

Technology Partner

ROMeo Process Optimization

romeo-process-optimisation_1

romeo-process-optimisation_2

Benefits

Evaluate “What-If” Scenarios

ROMeo Process Optimization provides a Microsoft® Excel-based and flow sheet-based interface to enable offline “what-if” scenarios, using precise models that represent your plant’s actual operating conditions. ROMeo models can also be used for procurement planning, and for evaluating the benefits of process changes.

Automate Optimization and Reporting

ROMeo’s Real-time System (RTS) provides an integrated, graphical scheduling environment that enables users to automate optimization and reporting. Using ROMeo’s RTS, users can easily define complex event sequences for closed loop optimization without user intervention. Task sequences can be scheduled to run daily, weekly, or at any preset interval. They can also be dynamically controlled when specific conditions, such as reaching steady state, are met.

Visualize Results and Key Performance Indicators

ROMeo’s industry proven results can quickly be visualized using embedded web page reporting and via the Wonderware® Intelligence application for web-based dashboards, displaying key performance indicators and other important operations information.

Product Attributes

Solutions for
Segment
Schneider Electric Certification