AVEVA InTouch HMI - Standard Edition

Visualise, Control and Optimise Your Operations
Published by AVEVA Group PLC

Features

  • Powerful Remote Access for Every User
  • Versatility and Extensibility
  • Powerful and Sophisticated
  • Ready to use symbol library
  • Situational Awareness for Operator Effectiveness
  • Unequaled Investment Protection

Powerful Remote Access for Every User

All casual and remote web HMI and mobile SCADA users can be empowered with AVEVA InTouch Web Client unlimited user license. This read-only web browser access to runtime InTouch graphics offers a low-cost delivery option for users that simply need production or process status monitoring, KPI access and operational dashboards. Moreover, the world’s favorite HMI is also fully mobile and works just about on any device including tablets and smartphones, with zero client installation and zero maintenance.

In addition, for Operators, InTouch Access Anywhere is an extension to AVEVA InTouch that provides full read write access to InTouch applications via any HTML5-compliant web browser. This offering fulfills our vision of enabling visualisation, collaboration and execution at various levels of the organisation. It enables users to securely monitor, control and troubleshoot plant equipment or processes from any location, on any device, at any time.

Versatility and Extensibility

AVEVA InTouch is an open and extensible HMI with intuitive graphical animation and scripting capabilities that provide incredible power and flexibility for application designers. AVEVA InTouch offers the ability to use vector graphics, bitmap graphics, library symbols, .NET controls and legacy ActiveX controls.

ArchestrA symbols support embedded .NET controls, giving you the freedom for unrestricted application extensibility without programming. They also offer access to standard controls such as Web browsers, desktop applications, mapping tools, ERP components and any other application based on .NET compliant controls.

Powerful and Sophisticated

Virtualisation technologies are key enablers for companies looking to save on hardware costs. No one in the industry offers more virtualisation options, including the latest Microsoft® virtualisation technology, Hyper-V and VMware. InTouch leverages Hyper-V and VMware so you can set up redundant HMI applications locally or at a remote site for more cost effective high availability and disaster recovery options 

Dynamic resolution conversion provides runtime scaling between screen resolutions, so you can view AVEVA InTouch applications on a variety of screen resolutions without having to modify the application. This enables operational agility with the ability the ability to build and run applications anywhere.

Ready to use symbol library

AVEVA InTouch comes equipped out-of- the-box with comprehensive library of pre-built, pre-tested stunning graphical symbols library and faceplates containing over 500 professionally designed ArchestrA graphic symbols, most with customisable ‘intelligence’ already incorporated, giving you drag-and-drop access to pre-built engineering components. 

AVEVA InTouch lower the engineering cost enabling you to quickly and easily develop custom graphical views of your real-time processes.

Situational Awareness for Operator Effectiveness

Through 30 years of countless visual and technological innovative advancements, AVEVA InTouch HMI brings unmatched clarity, consistency and meaning to integrated data. Collectively these visual innovations improve the ability to better understand the recent past, present and possible future of the process. 

The Situational Awareness Library of ArchestrA Graphics provides a superior set of building blocks for dynamic process visualisation. It's a unique resource that helps make it easier for operators to focus on the most useful content, troubleshoot and minimise distraction and fatigue. The result is less disruption and downtime and greater focus on performance improvement, safety and cost control.

Unequaled Investment Protection

With a thirty-year history of never leaving any customer behind, AVEVA InTouch consistently provides seamless upgrade path year over year that protects customer’s investments in AVEVA InTouch applications. An AVEVA InTouch application implemented decades ago can still run, unchanged, on the latest AVEVA InTouch software. You get all the benefits of the latest hardware and operating system improvements, without the re-engineering costs— no other company can make that claim. Simply the best HMI investment you can make.