Smart Connector - Oracle OPERA PMS Integration

Extension Enabling Communication between Oracle OPERA and EcoStruxure™ solutions
Published by Schneider Electric

Overview

Oracle OPERA PMS Integration

A Smart Connector PMS system interface that enables communication between Oracle OPERA (FIAS Protocol) booking system applications with EcoStruxure™ Platform. Based on OPERA, the leading enterprise solution suite for the hospitality industry.

Smart Connector - Oracle OPERA PMS Integration

EBO Integration

Benefits

Guest Arrival

Each room in the PMS is represented in the EWS model of the PMS. PMS attributes configured in the interface may be used to implement custom sequences. A multi state value indicates the number of persons checked into a room.

Guest Language

Using the language defined in the PMS for the checked-in guest, localization of the SE8000 Room Controller can enable the device to be set-up for the guests language preferences to optimise guest satisfaction.

Guest Departure Date

With knowledge of when the room is unoccupied or unrented, energy savings can be optimised by putting the room into a setback mode or energy savings control.

Product Evaluation

Claim your 30 day evaluation for this extension here (sign up required)

Download

Download the files required for this extension here

Product Attributes

Solutions for
Segment
Developer Resources
Domain
Unauthorised background image

Your product is just steps away!

Register for FREE to buy, get downloads and access free trials.

Get Resources and Start FREE Trials

Easy Product Activation with Your Account

Products Saved to Personal Digital Library