Features
Real programming using FBD (Functional Block Diagram) function block or contact language (LADDER)
Detection of any programming errors with its coherence test function
Simulation and monitoring modes: test the programme in real time, with or without the smart relay connected to the PC
Supervision windows: enables viewing of the I/O states of the smart relay in your application environment
Downloading and uploading of programmes
Edition of personalised files
Automatic compilation of programmes
On-line help