Unity DIF

Comparison software for EcoStruxure Control Expert project files
Published by Schneider Electric

Features

  • Highlights
  • Compare Unity Pro Applications

Highlights

  • Support for M580 and Momentum platform projects
  • New look and feel
  • Graphical representation of project differences
  • Supports XEF, ZEF, STU and STA file comparison
  • XML comparison for the selected section
  • Full Screen mode the maximize the application screen
  • Possibility to Print and Save the results
  • Comparison from Windows explorer context menu
  • Unity DIF V8.0 SP7 is compatible with Unity Pro V13.0, Windows 7 and 10 (32 and 64 bit) and Windows Server 2012 R2 (64 bit)
  • Unity DIF V8.0 SP7 is enhanced to support comparison of Modicon M580 Safety Projects in Unity Pro V13 XLS Note: It is not necessary to install Unity DIF V8.0 (or any version) prior to installation of Unity DIF V8.0 Service Pack 6
  • Quality Improvements
  • Compare Unity Pro Applications

    Unity DIF compares two Unity Pro application files (XEF, ZEF, STU and STA) and detects anything ADDED, DELETED and MODIFIED. The user interface and graphical representation of differences are similar to Unity Pro for consistency and ease of understanding the differences.

    Unity DIF can be launched in several ways:

  • From Unity Pro
  • From the Windows Start menu
  • From a command line interface
  • Unity DIF can provide differences for the following sections:
  • PAC Configuration (Hardware and Network)
  • Derived Data Types
  • Derived FB Types
  • Variables and FB Instance
  • Motion
  • Communication
  • Programs
  • Animation Table
  • Operator Screen
  • DTM Catalog
  • Project Settings
  • The result of the comparison can be printed or saved in .pdf and .txt file formats.