SCPTime BiaTime B
Published by
SCPTime
Features
time synchronisation traceable to legal UTC
BiaTime B is a Time-as-a-Service offer provided by SCPTime, which allows the user to synchronize their systems over internet traceable to official UTC time (from observatory of Paris). BiaTimeB can be used as an alternative or complementary solution to GPS or similar GNSS systems.
Hardware/software bundled service
BiaTimeB Service Package includes on-premise box(es), and a number of agents (depending on the edition of choice) to be installed on the end user devices to be synchronized.
plug and play
-
Plug and play installation of on-premise box (simple internet connection)
Holdover capacity
-
The on-premise box will ensure holdover capacity and continue to feed time signal in case of internet connection failure.
enhanced NTP protocol
Patented time protocol NTP STSĀ® to ensure time integrity and improve cybersecurity through network transfer.
Compatibility
-
Compatible with standard NTP
Full Traceability and compliance reporting
end to end traceability from official UTC time source (from Observatory of Paris) to user device. Supervision, alerts and edition of compliance reporting through user interface.
Continuity of Timing Service
Continuity of service on 24/7 basis
time synchronisation traceable to legal UTC
BiaTime B is a Time-as-a-Service offer provided by SCPTime, which allows the user to synchronize their systems over internet traceable to official UTC time (from observatory of Paris). BiaTimeB can be used as an alternative or complementary solution to GPS or similar GNSS systems.
Hardware/software bundled service
BiaTimeB Service Package includes on-premise box(es), and a number of agents (depending on the edition of choice) to be installed on the end user devices to be synchronized.
plug and play
- Plug and play installation of on-premise box (simple internet connection)
Holdover capacity
- The on-premise box will ensure holdover capacity and continue to feed time signal in case of internet connection failure.
enhanced NTP protocol
Patented time protocol NTP STSĀ® to ensure time integrity and improve cybersecurity through network transfer.
Compatibility
- Compatible with standard NTP
Full Traceability and compliance reporting
end to end traceability from official UTC time source (from Observatory of Paris) to user device. Supervision, alerts and edition of compliance reporting through user interface.
Continuity of Timing Service
Continuity of service on 24/7 basis